Major U.S. City Trusts “Battle Tested” Ames Backflow Preventers

 

What the Client Needed

Contractors in large cities commonly need to hurdle additional restrictions in comparison to suburban areas. When choosing a backflow preventer to install for the City of Chicago, a contractor from Assurant Fire Protection knows he needs a reliable product that meets all local mandates and restrictions.

Solution

The Ames Fire & Waterworks C500 is a Reduced Pressure Detector Assembly Backflow Preventer designed to prevent the reverse flow of fire protection system substances from being pumped or siphoned into the potable water supply. It incorporates a meter to detect ground leaks and unauthorized illegal taps, greatly reducing annual water expenses. The C500 is 70% lighter than traditional designs and is ideal for health hazard cross-connections, such as on fire sprinkler systems.

Other than the C500’s exceptional reliability, installers enjoy how simple maintenance is. “No matter which valve I choose (grooved, flanged, or N-pattern), the takeout is the same, making it easier to get inside there and work on it,” the Assurant Fire Protection contractor said.

Results

Currently there are thousands of C500s installed in Chicago with hundreds having been installed last year alone. “When I bring a C500 in, I never get any pushback,” said Assurant Fire Protection.

The battle-tested nature of Ames valves, combined with positive customer feedback and installation advantages, positions Ames as a trusted choice for fire protection in challenging urban environments. As cities continue to prioritize safety and compliance, Ames C500 stands out as a reliable and effective solution for fire protection infrastructure.

watts-logo

Share this Case Study

Location

Chicago, Illinois

Industry

Commercial

Category

Fire & Waterworks

Product(s) Installed

Ames Fire & Waterworks C500

Rep Agency

Mid-Continent Marketing

Contractor

Assurant Fire Protection
Assurant Fire Protection Contractor

When I put in a C500, I don’t need to worry about reliability. I can set it and forget it. I know when I test it next year, it will still be working smoothly.